Delete Reference Dynacard Data

Associated with: Dynacard Stores

Security permission required to access this pick action: Diagnostics

NOTICE

LOSS OF REFERENCE DATA

Use the Delete Reference Dynacard Data pick action with care. Once triggered, the pick action will permanently delete the ‘Reference’ data that is stored in ClearSCADA for the selected Dynacard Store.

Failure to follow these instructions can result in equipment damage.

Use this pick action to permanently delete the data that is currently stored as the ‘Reference’ data against which other dynamometer data is compared. Use the pick action, for example, if the existing set of ‘Reference’ data is misleading or inaccurate.

(To merely replace the existing set of ‘Reference’ data with more suitable data, you only need use the Copy a Stored Card to Reference Card pick action.)


Disclaimer

ClearSCADA 2017 R2