Monitoring the State of Direct Communications on your System

You can use Status displays to check on the status of individual channels or outstations (see Status Displays), and Mimics or Lists to monitor one or more channels or outstations on your system. Lists that display communication statistics, such as those listed below, are useful for monitoring the state of communications on a ClearSCADA system:

The Lists are available from the Queries Bar. For further information on using Lists, see the ClearSCADA Guide to Lists.


Disclaimer

ClearSCADA 2017 R2