Preparation

Before you can successfully configure an Outstation Set (other than PSTN), you need to have configured the channels that the outstations in the set are to use (see Configuring a Channel).

In order to do this, you need to be aware of the hardware setup on your system, as you need to configure the type(s) of set that correspond to your hardware setup. Therefore, you need to be aware of the type of communications used by the outstations in your system, and the channel(s) that those outstations use.

Configure your outstation sets to correspond to the communications structure of your system hardware.


Disclaimer

ClearSCADA 2017 R2