Show or Hide the Grid Lines

You can optionally display grid lines on an x-axis or a y-axis. The grid lines are a visual indicator that can make it easier to determine the values shown on the Dynagraph.

To display or hide the grid lines:

  1. Display the Dynagraph in Run or Design mode, as required (see Displaying an Editor).
  2. Right-click on the x-axis or y-axis, as required.
    A context sensitive menu is displayed.
  3. Either:
    • Select the Show Grid option so that it is prefixed by a check mark.
      The relevant grid line is displayed (a vertical line for the x-axis, or a horizontal line for the y-axis).
    • Clear the Show Grid option so that the check mark is removed.
      The relevant grid line is hidden from display.

Disclaimer

ClearSCADA 2017 R2