Size a Dynagraph According its Range of Data Values

You can use the Size to Data option to alter a Dynagraph’s magnification level. When used, ClearSCADA adjusts the magnification level so that the display includes the full range of the data readings that are available to the Dynagraph.

To adjust the magnification using this option:

  1. Display the Dynagraph in Run or Design mode, as required (see Displaying an Editor).
  2. Right-click on an axis or the main display area of the Dynagraph (the area that will contain the traces).
    A context sensitive menu is displayed.
  3. Select the Size to Data option.
    ClearSCADA alters the Dynagraph’s magnification level accordingly.

Disclaimer

ClearSCADA 2017 R2