Configuring Time Points

The ClearSCADA Advanced Modbus driver supports Time points.

Use a Time Point within the ClearSCADA database to retrieve a date/time value from a Modbus device (see Defining Time Point Details in the ClearSCADA Guide To Core Point Configuration).

Configure the properties of each time point using the fields on the Advanced Modbus Time Point Form.

This section covers configuration of properties on the Time Point tab of the Advanced Modbus Time Point Form. The properties on other tabs are common to points on many advanced drivers (see Tabs on Point Forms).

Use the Time Point tab to:

 


Disclaimer

ClearSCADA 2017 R2