Specify the Port Number to Communicate with a Remote Application

Use the Port field on the Connection tab to specify the TCP/IP port number that ClearSCADA uses to listen for commands from the application software.

The default is 49155. Specify the required number, typically in the range 1025 to 65535 (numbers 1 to 1024 are reserved for special use).

Where only one Remote Connection exists on a system, you can leave this setting at its default. Where multiple Remote Connections exist, specify a different Port number for each connection.


Disclaimer

ClearSCADA 2017 R2