Specify the Required Modbus Protocol and Packet Size

Use these fields on the Modbus tab to specify the type of Modbus protocol that the channel is to use and the maximum size of the data packets that can be transmitted via the channel:


Disclaimer

ClearSCADA 2017 R2