Advanced OPC Servers List

The Advanced OPC Servers List provides a summary of the status of the Advanced OPC servers to which your User Account and the client provide access.

As with other Lists, the Advanced OPC Servers List consists of rows and columns. Each row represents an individual server, and each column contains status information about the server.

The Advanced POC Servers List contains these columns:

As with other Lists, you can right-click on an entry in the List to display a context-sensitive menu. From this menu, you can select options to display further information about an OPC Server Report, or request various actions. For information on the actions that are Advanced OPC Server specific, (see Actions Associated with Advanced OPC Servers).


Disclaimer

ClearSCADA 2017 R2