Configure Analog Point Alarm Limits
This section describes how to use the fields within the Alarm Limits section of the Analog Point tab for analog points on the Advanced OPC driver, to set limits for a point and specify whether an alarm or event is generated if the point exceeds those limits.
Many of the Alarm Limits fields are common to many analog points (see Configure the Limits for an Analog Point).
For information on Hysteresis, see Specify the Hysteresis - the Minimum Value Change that can Clear an Alarm.
For information on the Engineering Units Exceeded field, see Define how Over Range and Under Range Values are Processed.
For information on Persistence Type and Persistence Duration, see Use Persistence to Stop Fleeting Changes in Value from Changing a Point State
For information on the Tune Limits feature, see Define whether an Analog Point’s Limits can be Tuned.
If the Area of Interest feature is enabled on your system, an Area of Interest field is displayed within the Alarm Limits section. For more information on this property, see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events.