Configure Private Security

Some OPC DA servers support Private Security, whereby you have to log onto the server in order to access the data. If this is required complete the following fields on the Server tab of the Advanced OPC DA Server Form:

Use the following fields to define whether OPC Private Security is used on the OPC server with which you want ClearSCADA to connect:


Disclaimer

ClearSCADA 2017 R2