Configuring a Radio Set on the Advanced Trio Diagnostics Driver
Much of the functionality and configuration that applies to Trio Radio Sets and Trio Radio database items is identical to that of Outstation Sets and Outstation database items in other ClearSCADA drivers. The core and generic ClearSCADA driver documentation uses the term 'outstation' to refer to devices such as outstations, data loggers, and radios from which ClearSCADA can retrieve data or control values. As such, you will come across the term 'outstation' rather than 'radio' in core topics and topics that are common to multiple drivers.
With the Advanced Trio Diagnostics driver, you use an Advanced Trio Diagnostics Radio Set to define a collection of Trio radios that share the same channel.
You configure the radio set in the database by using the fields on the Advanced Trio Diagnostics Radio Set Form. The Form includes a number of tabs.
You use the fields on the Trio Diagnostics Advanced tab to:
- Specify the Controller Address
- Specify Whether to Include the Stream Identifier in each Data Packet.
The other tabs on the Form, and the properties on those tabs. are common to channels on many drivers (see Tabs on Outstation Set Forms in the ClearSCADA Guide to Advanced Drivers).
Further Information
Configuring an Outstation Set in the ClearSCADA Guide to Advanced Drivers. (The Trio Radio Set is a Direct Set.)