Minimum Configuration

This topic relates to radios on the Advanced Trio Diagnostics driver.

When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:

 

For a radio on this driver to be capable of functioning in ClearSCADA, as a minimum you have to specify these properties on the item's configuration Form:

 

Also ensure that the radio and the database items on which it depends are In Service, and have saved, valid configuration. This will produce a radio that is capable of functioning using the default configuration settings.


Disclaimer

ClearSCADA 2017 R2