Points used on Advanced Trio Diagnostics Radios

With the Advanced Trio Diagnostics driver, you need to configure one Advanced Trio Diagnostics Point per item of diagnostics information that ClearSCADA is to retrieve from a Trio radio, or control that ClearSCADA is to send to a Trio radio.

The exception to this is where you have a hot-standby radio, in which case the number of points you require to represent 'shared' diagnostics data in the database varies, depending on the radio series. You require 1 set of points to represent 'shared' data in a D Series hot-standby radio, and 2 sets of points to represent 'shared' data in the other supported series of Trio radios (see Retrieve Data from a Hot-Standby Radio).

You need to configure points of the appropriate type to represent the type of data that you want the driver to retrieve or the output that you want the driver to control.

The driver supports these types of point:

You configure each point using the appropriate Advanced Trio Diagnostics Point Form. Each Form has several tabs.

The properties on each <Point Type> tab (such as the Digital Point tab on the Trio Diagnostics Digital Point Form) include:

The other tabs on the Forms, and the properties on those tabs, are common to points on many drivers (see Tabs on Point Forms in the ClearSCADA Guide to Advanced Drivers).

Further Information

Create a Point and Display a Point Form: see Create and Configure a Point in the ClearSCADA Guide to Core Point Configuration.


Disclaimer

ClearSCADA 2017 R2