Action Roster

An alarm redirection Action Roster allows you to configure a series of redirection actions that can trigger in a different order on different days, depending on your systems’ requirements.

Action Rosters are particularly useful if you require redirection actions to trigger only on certain days of the week, or during holiday periods, and so on.

If you use an Action Roster, you also need to configure the redirection actions that you want to use on the roster, or ensure that they exist on your system. You can attach any type of redirection action to an Action Roster.

For further information, see Configure an Action Roster.


Disclaimer

ClearSCADA 2017 R2