Move the Alarm Banner

If your User Account has the Can Move Banner feature enabled, you can choose whether to move the Alarm Banner to either the top or bottom of the ViewX or WebX window.

To move the Alarm Banner:

  1. Right-click on the Alarm Bell Button.
    A context-sensitive menu is displayed.

  2. Select the Dock Alarm Banner at Top option.
    The alarm banner will now display at the top of the ViewX or WebX window.

If required, you can move the Alarm Banner to the bottom of the ViewX or WebX window by repeating this procedure and selecting the Dock Alarm Banner at Bottom option instead of the Dock Alarm Banner at Top option.


Disclaimer

ClearSCADA 2017 R2