Confirm that the Required ClearSCADA Components are Installed

Before you can use Aquis with ClearSCADA you need to confirm that the Aquis components of ClearSCADA are installed on the ClearSCADA clients and servers.

On each ClearSCADA client and server on your system, use the Change function of the Programs and Features item in the Windows® Control Panel to see if the required ClearSCADA components are installed.

The required components are:

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2