Printing

ClearSCADA provides you with the facility to print a variety of data output. Aquis allows you to print any of the following:

To print any function that is displayed right-click the mouse
A context sensitive menu is displayed similar to that shown below.

Select the Print option.

Or:

Select CTRL + P from the keyboard.

The selected feature will be sent to your default printer.

Further Information

ClearSCADA's Printing facility


Disclaimer

ClearSCADA 2017 R2