Working with Views

Views allow you to change the display to show a predefined geographical area. Views are predefined within the Aquis application server for a specific region. The available views are listed in the View Bar.

Select the View you require, the Main view area changes to display the selected view. The content of the view is dependent on the Working with Themes selected. The Aquis Thin Client allows you to Using the Zoom Tool in and out within a selected view and select objects to display Accessing Object Data.


Disclaimer

ClearSCADA 2017 R2