Configure a Multi-Monitor Setup
To launch the ViewX Client on a Multi-Monitor setup, you need to create a Startup Configuration File.
The configuration file needs to be named 'StartupConfiguration.xml'and placed in the following directory:
C:\ProgramData\Schneider Electric\ClearSCADA
If this file is detected when the ViewX client launches, its settings are applied to the Multi-Monitor setup.
If the XML in the Startup Configuration File is not valid, a diagnostic message will appear when you launch the ViewX Client (see Resolve an Invalid Startup Configuration File).