Working with Single and Multiple Databases
A ViewX client can be configured to access a single ClearSCADA database or multiple ClearSCADA databases. Each ClearSCADA database is independent and runs as a ClearSCADA system on a ClearSCADA server (or on multiple ClearSCADA servers if used in a multi-server redundant architecture). This means you can use a single ViewX client to:
- Display information from one or more ClearSCADA databases
- Configure items in one or more ClearSCADA databases
- Issue controls to items in one or more ClearSCADA databases.
For more information on single and multi-database setups, please refer to the following sections:
A ViewX client can connect to a maximum of 64 databases.