Add a Data Set Row

You usually add one Data Set Row per 'normal' Group or Group Template (for a given Data Set).

To add a Data Set Row to the ClearSCADA database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the System, Group, or Group Template for which you want to add a Data Set Row.
    A context sensitive menu is displayed.
  3. Select the Create New option.
    A further menu is displayed.
  4. Select the Tables and Grids option.
    A further menu is displayed.
  5. Select the Data Set Row option.
    A Data Set Row is added to the root of the System or to the selected Group (depending on your selection in step 2). It is selected automatically, ready for you to enter its name.
  6. Enter a suitable name for the item (taking into account the ClearSCADA Naming Restrictions).
  7. Press the Enter key or select another part of the ViewX interface to confirm the entry.

Disclaimer

ClearSCADA 2017 R2