Column Headings for other Types of Filtered Value Map

Filtered Value Maps other than Filtered BIT Value Maps and Filtered String Value Maps contain the same column headings as Value Maps (see Column Headings for other Types of Value Map), plus these additional column headings:

The four deadband limits are used within each Filtered Value Map to indicate whether a change in value has caused a change in state—if so, this is stored as an alarm at the Value Map, and is reported to the Master as part of the ‘reasons for change’ for that value. You can specify four deadband limits:

These column headings are also displayed for each Filtered Value Map:


Disclaimer

ClearSCADA 2017 R2