Define the Severity Type

In some instances, you can define whether ClearSCADA is to log an event or raise an alarm under specific circumstances. For example, you specify whether ClearSCADA is to trigger an alarm or event when a point enters a particular point state. (For more information on configuring point states and alarm limits, see the relevant ClearSCADA configuration documentation.)

You specify whether an alarm or event is to be triggered, by using the Severity fields on the appropriate Form. In this case, two Severity fields are displayed—one to define the type of activity that is to be triggered (for example, an event), and the other to define the priority for that activity.

Use the combo box on the first Severity field to display a list of severity types. Choose the option that you require:

The second Severity combo box does not display a ‘None’ option, as the box becomes ‘grayed out’ (unavailable) if ‘None’ is selected from the first Severity combo box.

The second combo box’s default options can be overwritten by a custom range of priorities. If the default settings in the second Severity combo box have been replaced by a customized range, select the appropriate level of importance. (For information on changing the default settings, see Alarm and Event Severities in the ClearSCADA Guide to Server Administration.)

If the Dictionary feature is used on your system, strings in the second Severity combo box may be prefixed with @, in order for those strings to be replaced with other terms, when displayed in a List or on a Mimic, in ViewX. For more information, see Introduction to the ClearSCADA Translation Dictionary in the ClearSCADA Guide to the Translation Dictionary.

Example:

The diagrams in this example show how the Severity settings might be configured for a digital point.


Disclaimer

ClearSCADA 2017 R2