Edit an Existing Field

To edit a field on a Data Table:

  1. Display the Data Table in Design mode (see Edit a Data Table).
  2. Right-click on the field.
    A context sensitive menu is displayed.
  3. Select the Properties option.
    The Edit Field window is displayed.
  4. Use the window to Specify the Field Properties.

Disclaimer

ClearSCADA 2017 R2