Master Station Override


Associated with: Points

The Master Station Override state is indicated by a blue background color, by default.

The color indicates that the data for a point has been overridden at the master station.

Operators with the required permissions can override a point if the Override feature has been enabled on the configuration Form for that point.

Also see Outstation Override.


Disclaimer

ClearSCADA 2017 R2