Reorganize the Areas of Interest on your System

You can reorganize the Areas of Interest on your system, however this procedure should be used with care. If you move an Area of Interest from one location to another:

To move an Area of Interest from one location to another:

  1. Display the Areas of Interest Bar.
  2. Select the relevant entry in the Areas of Interest Bar. Do not release the left-hand mouse button.
  3. Drag the cursor so that it is positioned over the Area of Interest within which you want to move the selected entry.
    The target Area of Interest is highlighted.
  4. Release the left-hand mouse button.
    The entry is moved into the target Area of Interest.

Disclaimer

ClearSCADA 2017 R2