Reset

Associated with: Master Station Accumulators that use a Continuous reset method

Security permission required to access this pick action: Control

With an Accumulator that is configured to use a Continuous reset method, ClearSCADA automatically sets that Accumulator’s value back to zero at the end of each calculation period (see Specify the Period over which an Accumulator’s Value is Calculated).

If required, you can use the Reset pick action to reset an Accumulator’s value to zero, independently of the End of Period Reset settings configured for that Accumulator.

Further Information

Continuous reset method: see Specify whether an Accumulator Continuously Sends Timed Reports and Resets its Value.


Disclaimer

ClearSCADA 2017 R2