Source Refresh

Associated with: Simple driver point sources (for example, scanners)

The Source Refresh state is indicated by a flashing blue foreground color, by default.

The color indicates that a Refresh is in progress. A Refresh can be triggered automatically, or manually using the Refresh pick action. If necessary, an ongoing Refresh can be canceled by using the Cancel Refresh pick action.


Disclaimer

ClearSCADA 2017 R2