Specify the Profile’s Range
Use the Minimum and Maximum fields within the Range section of the Profile tab to specify the range of values that the Profile can display.
A Time Profile has a ‘normal’ scale if its Maximum value is greater than the Minimum value.
A Time Profile has an inverted scale if its Maximum value is less than the Minimum value. (A Time Profile that is used for alarm limits on analog point(s) that have inverted scales must itself have an inverted scale.)
- Maximum—Enter the maximum value that the Profile can display.
- Minimum—Enter the minimum value that the Profile can display.
If you reduce the range of an existing Time Profile, ClearSCADA will automatically move any out-of-bounds vectors to the new Minimum or Maximum value, as appropriate.
If you Produce a Profile Based on Historic Data and any of the values exceed the Profile’s Range, ClearSCADA will substitute any larger values with the Profile’s Maximum value, and any smaller values with the Profile’s Minimum value (or vice versa if the Profile has an inverted scale).
If the SetVectors method is used to Generate a Profile’s Data Programmatically and any of the values exceed the Profile’s Range, the method will not succeed.