Text String Syntax

The syntax for text strings is given below:

Code Description

>

Forces the whole string to appear in upper case

<

Forces the whole string to appear in lower case

Example:

The syntax > is used to force the incoming string value ‘Xerox 123’ to be displayed within ClearSCADA as ‘XEROX 123’.

The syntax < is used to force the incoming string value ‘Printer TRAY 5’ to be displayed within ClearSCADA as ‘printer tray 5’.


Disclaimer

ClearSCADA 2017 R2