Using the Add Action and Edit Method Windows
You use the Edit Method window, the Add Action window, or the Edit Action window to select a method (action) that ClearSCADA is to trigger automatically, and to specify the values of any arguments used by that method.
Although the name of each window varies, depending whether you access it via a Form or a Schedule, much of the functionality of each window is the same. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.