Using the User Methods Tab to Define Custom Actions
You use the User Methods tab on the relevant configuration Form to specify the database item with which an action is to be associated and the ‘method’ that ClearSCADA is to trigger on that item. You also use the tab to specify a custom title for the pick action (see Add a Custom Pick Action).
Once configured, the custom action is automatically appended to the list of ‘core’ and driver-specific pick actions for that item.
For a series of examples that demonstrate how custom actions might be used on a ClearSCADA system, see Example Configuration.