Define the Format of a Digital Point’s Values

You can use the Format field on the Digital Point Form to define the appearance of a digital point’s values. The Format field is displayed on the Digital Point tab.

The format that you choose will determine how the digital point’s value is shown on other displays, such as Lists and Mimics.

To define the format of the digital point’s values:

  1. Display the Digital Point Form for the digital point that you want to configure (see Display a Form in the ClearSCADA Guide to Core Configuration).
  2. Select the Digital Point tab.
    (If you are configuring the format for another point that uses digital-type processing, select the appropriately named <Point Type> tab.)
  3. Select the browse button next to the Format field.
    The Text Format window is displayed.

  4. Use the Text Format window to choose and define the required type of formatting (see Choose a Format Category in the ClearSCADA Guide to Core Configuration).
  5. Save the configuration (see Saving Configuration Changes in the ClearSCADA Guide to Core Configuration).

Disclaimer

ClearSCADA 2017 R2