Defining String Point Details

Use a String Point within the ClearSCADA database to represent an internal point, or to retrieve or set the value of a property on another device or application, when that property has a textual string value, rather than a numeric value. For instance, to retrieve information on the present status of a printer that is attached to the system.

Configure each string point on your system by using the fields on the String Point Form. The Form has several tabs, which you use to define different aspects of point configuration. This section explains how to configure point properties that are common to many string points. You configure most of these properties on the String Point, Control and Manual tabs of the appropriate String Point Form.

Use this section, along with the appropriate driver documentation, for information on configuring the string points on your system.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

(In addition to internal string points, ClearSCADA also supports String Parameters and String Variables. The type of string that you add to ClearSCADA depends on the string’s intended functionality. For more information, see Parameters versus Points and Variables in the ClearSCADA Guide to Core Configuration.)


Disclaimer

ClearSCADA 2017 R2