Define the Historic Storage of a Report

Use the fields on the Historic tab to specify whether the server is to store reports historically.

The Historic tab is only included on the relevant configuration Forms when the Historic Files feature is enabled on the server. The Historic Files feature enables ClearSCADA to store files such as reports historically (see Enable or Disable Historic Files).


Disclaimer

ClearSCADA 2017 R2