Status
Associated with: Crystal Reports
This attribute indicates the present status of any activity associated with a report, such as a request to export, print, or generate a report.
Possible States:
- Idle—ClearSCADA is not actively processing any requests associated with, and there are no requests outstanding for, this report. The last request associated with the report was executed successfully.
- In Progress—ClearSCADA is actively processing a request associated with this report. For example, a request to generate the report.
- Pending—A request associated with this report is pending (as ClearSCADA is presently processing request(s) for other items). This state will change to ‘In Progress’ when a thread becomes available for use.
- Failed—The last request associated with the report failed. Refer to the Events List for further information about the failure (for example, an Export request might fail if the export destination cannot be reached).