The Server Fails to Generate a Report

Reports are generated using the Generate Report pick action.

If report generation fails, a diagnostic message appears in the Status bar and is logged in the Event Journal. The diagnostic message summarizes the reason that the server failed to generate the report.

If the reason that the report failed to generate is due to logon failure, check that:

If the reason that a report failed to generate is due to a missing table, check that the table(s) that the report references do exist in the database. An error occurs if an attempt is made to generate a report that references a non-existent database table (for example, a custom table such as a Historic View, that has not been configured on the server).

Within ClearSCADA, this type of message is displayed:

‘Generate report request failed - Failed to generate report, the table “ could not be found...’


Disclaimer

ClearSCADA 2017 R2