Specify the Clock Alarm Severity
You can specify the importance (severity) that you want to attach to alarms that are associated with setting the outstation's clock. To do this, you use the Set Clock Alarm Severity combo box on the DNP3 tab.
Use the combo box to select a severity level. You can select from None, Low, Medium, High or Critical.
Further Information