Device Serial Number

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve System Overview information.

This status attribute indicates the number of Data Carrier Detect (DCD) drop outs that have occurred on the port.

This attribute applies to SCADAPack ES and ER models only.

Example:

4125


Disclaimer

ClearSCADA 2017 R2