Firmware Upgrade Alarm

Associated with: DNP3 SCADAPack E outstations, other than DNP3 SCADAPack Remote DNP3 Devices.

This status attribute indicates whether ClearSCADA’s last attempt to Download Firmware or Download Remote Firmware was unsuccessful.

An existing firmware upgrade alarm is cleared when ClearSCADA next updates the operating system firmware successfully.

Possible States: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R2