ISaGRAF App n Start Time

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve System Overview information

Two Start Time attributes are displayed for each ISaGRAF application (1 and 2).

The first status attribute indicates the date and time at which the currently loaded ISaGRAF application started to run, decoded into a text string.

Example:

May/08/2009 12:20:07.591

The second status attribute displays the raw number that was returned by the outstation, indicating this start time.


Disclaimer

ClearSCADA 2017 R2