Internal Battery Low

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve SCADAPack ES Remote I/O information.

This status attribute indicates whether the on-board battery’s power is running low.

Possible states: True, or False.

Do not confuse this status attribute with the Input Power Low attribute.


Disclaimer

ClearSCADA 2017 R2