Specify when a Change in Value Triggers a Change in Point State

The following fields are displayed toward the bottom of the Alarm Limits section on the Analog Point tab:

The Persistence into/out of Alarm properties are only relevant if the point has a Point Data Class of Class n Event (see Configure Common Properties of DNP3 SCADAPack Points).


Disclaimer

ClearSCADA 2017 R2