<Status Information Item> Quality

Associated with: DNP3 SCADAPack Status Information items.

This status attribute indicates the reliability of a specific item of status information data. <Status Information Item> indicates the item of data to which the attribute refers.

A set of status attributes is displayed for each item of status information that ClearSCADA retrieves from a DNP3 SCADAPack E outstation or remote I/O module.

Use the attribute in conjunction with the <Status Information Item> Update Time attribute to ascertain the reliability of that particular item of status information.

For a comprehensive list of possible Quality values, see Quality in the ClearSCADA Guide to Drivers.


Disclaimer

ClearSCADA 2017 R2