TCP/IP Routing

You can configure a SCADAPack E outstation to route TCP/IP packets between multiple networks.

The outstation is capable of routing between Ethernet and Serial (PPP) on multiple interfaces.

 

Further Information

Use an IP Route Table to Route TCP/IP Packets to Another TCP/IP Host.

Enable TCP/IP Services.

Configure TCP Service Port Properties.


Disclaimer

ClearSCADA 2017 R2