Trend Retrieval Alarm

Associated with: DNP3 SCADAPack E outstations, other than DNP3 SCADAPack Remote DNP3 Devices.

This status attribute indicates whether ClearSCADA’s last attempt to retrieve sampled trend data from the outstation was unsuccessful.

A request to retrieve such data might be initiated:

Possible states: Displays one of the Standard Alarm States.

An alarm state indicates that the last request to instruct the outstation to create a Trend log, retrieve a Trend log, or delete a Trend log after the file has been read, was unsuccessful. Should an alarm state occur, ensure that there are no problems with communications to the outstation. If large amounts of data regularly need retrieving, or the link to the outstation is slow or heavily utilized, timeouts might occur. If such timeouts occur regularly and are not due to equipment failure, modify the configuration.


Disclaimer

ClearSCADA 2017 R2