Upload Config

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations

Security permission required to access this pick action: Retrieve Data

Use the Upload Config pick action to cause:

The generated file contains the complete configuration of the outstation, excluding:

The resulting file can be opened using the E Configurator, to examine the configuration of the SCADAPack E outstation.

If using this pick action with the Automation Interface (see DNP3 SCADAPack E Automation Interface Methods), you need to specify the method name eNETUploadConfig.

Also see Import Firmware Image.


Disclaimer

ClearSCADA 2017 R2