Access the Database Schema
You need to use Internet Explorer to access the ClearSCADA Database Schema. You can then use the ClearSCADA Database Schema to locate information about the classes.
To access the ClearSCADA Database Schema:
- Run Internet Explorer on any PC in the network.
- In the Address field, overwrite any existing address with:
http://<server name>:<web server port>/Schema
Where:
-
<server name>
is the name of one of your ClearSCADA servers <web server port>
is the HTTP port number that is defined in the WebX section of the ClearSCADA Server Configuration Tool (see Define the Ports Settings for WebX Clients in the ClearSCADA Guide to Security).
Do not enter the angle brackets <>.
Alternatively, if you are using the server PC and it uses port 80 for the web server's port, you can enter:
http://localhost/Schema
-
- Press the Enter key or select the Go button.
The ClearSCADA Database Schema is displayed.