Alarm Limits

Associated with: Analog and Counter-type points for which alarm limits are currently tuned

This status attribute is only displayed for points on which:

The attribute lists:

With points on some drivers, you can associate individual limits with Time Profiles. Profile-controlled limits cannot be tuned. If any limits are tuned on a point on which other limits are profile-controlled, the Alarm Limits status attribute indicates which of those limits are profile-controlled.

Example:

Tuned to HH:95.00 H:Profile L:25.00 LL:10.00 by RGrosso at 29/Nov/2007 14:09:22.648

Also see M/S Alarm Limits.


Disclaimer

ClearSCADA 2017 R2